how to use Serial1 on Artemis nano?

paulvha:
Given that someone else also complained about Serial speed setting I have bought an Artemis Nano.

Compiled your example and … now I got the same problem as you. I could not set the speed for Serial and Serial1 independent from each other and the data is showing up BOTH on Serial as well as Serial1.

I have been able to find the root cause and solution.

An Apollo3 chip has 2 uarts : UART0 and UART1. When a Serial instance is created, based on the provided TX and RX pad, a lookup is performed to decide which UART to use.

First, the Serial-instance is created (TX = 48 / RX= 49) and based on the lookup UART0 is assigned. Then the Serial1-instance is created (TX=39, RX =40), but now DUE TO AN ERROR IN THE LOOKUP TABLE, it is ALSO assigned to UART0.

In the same lookup table (PeripheralPins.c) there are already entries to assign (TX=39, RX =40) to UART1. So I commented-out the 2 lines that enable UART0 assigment. Serial1 is now assigned to UART1 and it now works as expected.

The change requires a new Artemis-Nano pre-build archive for Mbed, which I have created.

Go to  the directory :

Windows : \AppData\Local\Arduino15\packages\Sparkfun\hardware\apollo3\2.2.1\variants\SFE_ARTEMIS_NANO\mbed

Ubuntu/Linux:~/.arduino15/packages/SparkFun/hardware/apollo3/2.2.1/variants/SFE_ARTEMIS_NANO/mbed

There is the archive file called libmbed-os.a.
If you want you can make a safety rename or copy.

Now UNZIP the attached libmbed-os.zip in this folder to get a updated an libmbed-os.a and recompile your sketch .
All should be working now.




Note 1: Why I did not see this on any of the other boards ? Because they use TX=24 / RX=25 for Serial1, which in the table can only be assigned to UART1.



Note 2: I have made a github bug report : [https://github.com/sparkfun/Arduino_Apollo3/issues/474](https://github.com/sparkfun/Arduino_Apollo3/issues/474)

There might be a bug in this build that causes the BLE address to become fixed. I was experiencing the glitch where multiple Artemis units have the same BLE MAC address and muscle each other out of the way and leave it random which device I’m connecting to, and when I ran the same code on another PC that seemingly didn’t have this fix, the BLE MAC problem was cleared up.

Correlation doesn’t necessarily mean causation, but I thought I’d bring it up