The red-v board uses a sifive fe310 cpu.
The cpu lists in its memory map that it has an i2 controller located at $10016000.
Does programming this controller also program the qwiic connector?
The red-v board schematic shows a section labeled “Headers”.
In this section JP2 shows that the blue LED is located at 5 and the LED can be addressed as GPIO pin 5.
JP2 also shows sda/1 and scl/1. Are these pins used for the i2 qwiic connector? Do we use GPIO pins 1 - 4 to program /power up the qwiic connector?
Thanks for any help