Hi guys,
So my project is basically a motor that rotates a pully very slowly (30-40rpm) until a force sensitive resistor is touched. When the fsr senses the force the motor will stop Rotating. The motor will have to be in the 200-400kv range for the torque I’m looking for. Would I need an arduino motor shield or esc for my motor on this project?
How do you think I should wire this? My initial guess was an arduino uno with a motor shield and 10kOhm resistor connecting to the fsr, with the motor connected to the shield.
Thanks in advance for any help!