Hi, first time trying to use relays.
Got this PCB: http://www.sparkfun.com/products/9096
All components are as the PCB tells me.
When I connect the board to my arduino uno I can only see a very dim blink on the diod and no click sound from the relay.
Code: digitalWrite(7, HIGH); //connected to CTRL pin
Connected GND to arduino GND
and 5V to 5V
If I connect the CTRL pin to 5V the relay works
Is the current to low from the arduino pin7 to controll the relay board?!?!
I power the Arduino from USB and I tried external 5V aswell (1A)
What should I try or fix, iam stuck.