I have some problems with lpc2478 ~ please help me ~ thx

problem 1. (board : olimex-lpc2478)

The IAR software show the message "Fatal Error[Pe005]: could not open source file “nxp/iolpc2478.h”

Could you please tell me where I can find or download “nxp/iolpc2478.h” ?

===============================================

problem 2. (board : olimex-lpc2478)

Why can the mmc card not load linux and romfs ?

The u-boot show the message :

mci-cid (SD memory card):

Manufacturer ID: 0x1b

OEM/Application ID: SM

Product Name: SMI

Product Revision: 1.0

Serial Number: 0x000c27ae

Date Code: 2007.11

sector size = 512 (Bytes), card size = 510 (MBytes)

dump csd data: 005e00325f5983cc

edb77f8f9640007c

mmc_block_read: start=0, blkcnt=1

The u-boot does not work after showing the message.

Even if I key in “0” or “1” .

Could you please tell me the reason ?

==============================================

problem 3. (board : LPC2478 QVGA Board Bundle = EA-OEM-203 =Embedded Artists)

I try to use the software LPC2xxx-gcc-newlib v2.4.0.1 to load u-boot.hex or uClinux.hex to board,

example : lpc21isp test.hex com5 38400 12000

but the software show the message " no answer on ‘?’ " after finishing loading.

Could you please tell me what the reason is ?

Or you have the other good methods to provide me.

sorry~my English is not very good .

Please help me .

Thank you for your help~very grateful.

The iolpc2478.h fule is available when you purchase the IAR 2478 starter kit. Did you purchase it? If so, it should be part of the installation in the IAR directory.

Hello,

I can’t find the iolpc2478.h in the IAR directory.

Why ?

Can you tell me the reason ?

Or you can mail the iolpc2478.h to me.

Thank you for grateful .

Hello ,

have you check C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\inc\NXP\ (assuming standart installation) ?

your choice of microprocessor target in the project settings should resolve all the chip related .h files automatically.

I use IAR EWARM-EV-WEB-511 now.

I can’t find the iolpc2478.h from C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\inc\NXP\ yet.