Hello everyone, I need help with my school project.
In my physics class, we are learning how to use arduino to help us understand physics.
Basically, we have an aluminum bar and we are trying to explain why a neodymium magnet goes down slower than an iron ball inside it.
And I’m supposed to program LEDs to turn on (using LDRs) everytime the ball passes through it and write down the seconds, but I can’t use others hardwares, only the serial monitor.
Hardware: 6 LDRs, 6 LEDs and an aluminium bar
So, here is what I need to know:
1- How can I make serial monitor show every 6 LDRs values in every second?
2- I need to program it to write down the seconds in the serial monitor everytime the ball passes through.
Here is what I have so far, it isn’t right, but it’s a start.
int LED1 = 13;
int LED2 = 12;
int LED3 = 11;
int LED4 = 10;
int LED5 = 9;
int LED6 = 8;
int LDR1 = A0;
int LDR2 = A1;
int LDR3 = A2;
int LDR4 = A3;
int LDR5 = A4;
int LDR6 = A6;
int val1;
int val2;
int val3;
int val4;
int val5;
int val6;
void setup (){
pinMode (LED1, OUTPUT);
pinMode (LED2, OUTPUT);
pinMode (LED3, OUTPUT);
pinMode (LED4, OUTPUT);
pinMode (LED5, OUTPUT);
pinMode (LED6, OUTPUT);
Serial.begin (9600);
}
void loop(){
val1 = analogRead (LDR1);
Serial.println (val1);
delay (1000);
if (val1 > 50){
digitalWrite (LED1, HIGH);
}
else if (val1 <= 50){
digitalWrite (LED1, LOW);
}
val2 = analogRead (LDR2);
Serial.println (val2);
delay (1000);
if (val2 > 50){
digitalWrite (LED2, HIGH);
}
else if (val2 <= 50){
digitalWrite (LED2, LOW);
}
val3 = analogRead (LDR3);
Serial.println (val3);
delay (1000);
if (val3 > 50){
digitalWrite (LED3, HIGH);
}
else if (val3 <= 50){
digitalWrite (LED3, LOW);
}
val4 = analogRead (LDR4);
Serial.println (val4);
delay (1000);
if (val4 > 50){
digitalWrite (LED4, HIGH);
}
else if (val4 <= 50){
digitalWrite (LED4, LOW);
}
val5 = analogRead (LDR5);
Serial.println (val5);
delay (1000);
if (val5 > 50){
digitalWrite (LED5, HIGH);
}
else if (val5 <= 50){
digitalWrite (LED5, LOW);
}
val6 = analogRead (LDR6);
Serial.println (val6);
delay (1000);
if (val6 > 50){
digitalWrite (LED6, HIGH);
}
else if (val6 <= 50){
digitalWrite (LED6, LOW);
}
}
I’m new to programming, that is why I need help. If you can help me, I will be very thankful. ![]()