Hello ! ![]()
I am trying to use the Battery Babysitter:
https://www.sparkfun.com/products/13777
with a PIC 16F18875.
I have the arduino library to help me but I need to adpat it to my PIC.
https://github.com/sparkfun/Battery_Bab … Q27441.cpp
So the arduino using c++ and pic is C so I removed the class part of the code. I could reuse all the functions except the last 2 ones that are being use from all the others :
// Read a specified number of bytes over I2C at a given subAddress
int16_t BQ27441::i2cReadBytes(uint8_t subAddress, uint8_t * dest, uint8_t count)
{
int16_t timeout = BQ72441_I2C_TIMEOUT;
Wire.beginTransmission(_deviceAddress);
Wire.write(subAddress);
Wire.endTransmission(true);
Wire.requestFrom(_deviceAddress, count);
while ((Wire.available() < count) && timeout--)
delay(1);
if (timeout)
{
for (int i=0; i<count; i++)
{
dest[i] = Wire.read();
}
}
return timeout;
}
// Write a specified number of bytes over I2C to a given subAddress
uint16_t BQ27441::i2cWriteBytes(uint8_t subAddress, uint8_t * src, uint8_t count)
{
Wire.beginTransmission(_deviceAddress);
Wire.write(subAddress);
for (int i=0; i<count; i++)
{
Wire.write(src[i]);
}
Wire.endTransmission(true);
return true;
}
My problem is with wire library. I have my I2c functions for a PIC Write(data), read() ,stop(), start() ,init(), acknowledge,nacknowledge.
Do you think I can replace the beginTransmission with a init a start and a write(adresss) ?
Same for endtransmission(true) with a stop ?
And for requestFrom and available I have no idea how to do it. Here are the code for them in Arduino
Requestfrom :
Used by the master to request bytes from a slave device. The bytes may then be retrieved with the available() and read() functions.
Available:
Returns the number of bytes available for retrieval with read(). This should be called on a master device after a call to requestFrom() or on a slave inside the onReceive() handler.
My question is how to delete the wire. functions and replace them with my PIC I2C functions
Thank you for the help
uint8_t TwoWire::requestFrom(uint8_t address, uint8_t quantity, uint32_t iaddress, uint8_t isize, uint8_t sendStop)
{
if (isize > 0) {
// send internal address; this mode allows sending a repeated start to access
// some devices' internal registers. This function is executed by the hardware
// TWI module on other processors (for example Due's TWI_IADR and TWI_MMR registers)
beginTransmission(address);
// the maximum size of internal address is 3 bytes
if (isize > 3){
isize = 3;
}
// write internal register address - most significant byte first
while (isize-- > 0)
write((uint8_t)(iaddress >> (isize*8)));
endTransmission(false);
}
// clamp to buffer length
if(quantity > BUFFER_LENGTH){
quantity = BUFFER_LENGTH;
}
// perform blocking read into buffer
uint8_t read = twi_readFrom(address, rxBuffer, quantity, sendStop);
// set rx buffer iterator vars
rxBufferIndex = 0;
rxBufferLength = read;
return read;
}
int TwoWire::available(void)
{
return rxBufferLength - rxBufferIndex;
}