Ideas for when shipping items or on the site.

Most people are kind of new to the whole I have a chip what do I do now.

I would suggest like a step by step guide on how to hook it up to the programmer and maybe some links to the programs you might need to use to program the chip. Also one or two easy asm that provide the board works and such.

The reason I say that is because I got the Transceiver Development Kit and I was like ok now what. Then I downloaded the spec sheets and still didn’t get any ideas on what to do. But after much trying I finally got the serial cable to the convertor board thing to plug into the 2.4g evk board, but I don’t unserstand how to program or if I can program the other chip with the antenna’s. So you can see were this is a little frustrating and the foums are minimal help, along with the tutorials.

So to wrap up. Every project should have a get started guide. 1) download these programs. 2)plug this into that. 3)Program it this way or that and here are some sample codes. This would be awesome.