I’m currently working on an IIR-filtering function-set and though it works, I find it a little time demanding for my SAM7.
I run the core-clock at about 55 MHz, and I have timed one filter update to 5.5 µS. This is for an order 4 filter.
Well, it might sound quite fast, but in fact it takes 300 clock cycles.
I have written my own fixed-point math routines, which I have checked does not use more than a single SMULL-instruction and a shift to do a multiplication.
So the pseudo code for one filter update is something like this:
A and B are the pre-generated nominator and denominator for the filter.
inbuffer[0] = inbuffer[1];
inbuffer[1] = inbuffer[2];
inbuffer[2] = inbuffer[3];
inbuffer[3] = in_signal;
sum = inbuffer[0] * B[0] +
inbuffer[1] * B[1] +
inbuffer[2] * B[2] +
inbuffer[3] * B[3] -
feedback[0] * A[0] -
feedback[1] * A[1] -
feedback[2] * A[2];
feedback[0] = feedback[1];
feedback[1] = feedback[2];
feedback[2] = sum;
signal_out = sum;
Of course, my routines are a little more structured, but they are inlined so it should compile into something very similar to this. Should this really take 300 cycles to execute?![]()