Hey guys, I’ve done abit of reading on the site to try and find out an answer to my question, but alot of it goes too deep for me… Im 22, avionics technician, and can handle abit of techo lingo, my problem appears to be from the reciever side of things.
I have a 16f84 simply incrementing a 4 bit word and then setting a pin low for one cycle to enable TX from the ht12e, then allowing 1/100 of a second(should be lots of time for a 3Kosc set on the ht12e/d to send one word).
However… always a however for my projects… the ht12d recieves data here and there - the first few words are right on the ball, then it appears like the decoder gets out of synch… bad juju…
The data is TX/ing fine, i have a LED on the signal out line to the RF tx’er(TLP 433Mhz) and its flashing away doing its thang, but the ht12d on the RX is not getting the data… I have a LED on the data line from the RLP on the receiver and there appears to be alot of noise when the TX isnt even transmitting, on that I tried moving the board around the house to see if it was jsut the room i was in, but it wasnt. The LED flashes dimmly with no TX, I would have thought that it would stay off(0v) with no data being recieved…
Anyhow, one last thing, even though the data is being sent at around 3K as definned by the RLP/TLP and ht12d/e Fosc settings, why is it that i cant seem to get data transfer nealry as fast, is the 3K bits per second or bytes per second?
Thanks in advance guys, after reading some of the other forums out there its really got me thinking about new projects and designs, but hey, gotta start somewhere ![]()