IMU SENSOR IS NOT WORKING ON SURVEYMASTER APK. RTK EXPRESS PLUS

AS THE GUIDE SAYS, I HAVE CONFIGURED THE RTK TO WORK WITH THIS APP BUT IN THE INTERFACE OF THE APP I CANT USE THE OPTION TO GET POINTS WITH THE IMU, I ALREADY ENABLED THE IMU SENSOR THROUGH THE WIFI CONFIG BUT NOTHING HAPPENED CAN SOMEONE HELPME WITH THAT?

Could you recommend me a software to use the rtk with the imu function? Cause sw maps and surveymaster are recommended on the main page, but neither can use the imu

Hi VictorJim05 - Sorry for the confusion but the IMU in the RTK Express Plus is only used for automobile applications to maintain positioning when GNSS reception is degraded or lost. The IMU is not available for tilt compensation. I’m sorry if the product description was not clear enough.

We’ve been asking u-blox to enable tilt compensation in the ZED-F9R (the GNSS receiver in the RTK Express Plus) but up to this point, they have not be able to add it.

Is it possible in the meantime?
I bought the Sparkfun RTK express Plus with the same intention

Hi @JoGe ,

Just cross-linking to your second post. Apologies for the slow reply here.

Best wishes,
Paul