Dear OpenOCD Users,
i would like to use the olimex gccfd development suite.
The problem is that i do not have enough space available
on my C-Drive and want to install the programm on
e.g. L:\ARM.
I did not found out how this is working?
Option /D=L:\ARM did not work.
I would be very pleased if anyone could help me.
Thank you very much in advance.
Best Regards
Christoph
mifi
2
Hello Christoph,
what do you mean with gccfd?
Do you use the ARM-USB-OCD?
Best regards,
Michael
Hello Michael,
i have a dev-board for the LPC2103F from SILICA.
There is included a GCC-compiler, Eclipse and OpenOCD.
It is called “Olimex’s ARM-JTAG-OCD GCC for Dummies”.
For debugging the ARM-USB-OCD might be used.
To install the compiler, Eclipse and OpenODC there is
one install programm (OLIMEX-GCCFD-141206.exe)
on the CD included. This installs all the programms
on the C-Drive. The install program for the software-
package is Nullsoft Install System 2.20
There is no posibility to chose the installpath during
the installation procedure.
I found some hints at Nullsoft for command-line
installationi options but it did not work.
Perhaps someone here in the forum did work with
the programm already and could help me.
Regards
Christoph
mifi
4
Hello Christoph,
take a look here: www.yagarto.de
Perhaps this will help you, here you will find everything you need to start.
Even you will find some how-to’s. By the installer you can set the
directory you like.
I know the ARM-USB-OCD cd, I belive that WinARM is used here,
WinARM can be found here too:
http://www.siwawi.arubi.uni-kl.de/avr_p … ts/#winarm
Best regards,
Michael