Hi
I’m a student and trying to setup a small project at school and desperatly need some help with this
My plan was to do the following:
controlling street lights where I want to include a sensor (radar motion detector) in each lightpole, the lightpole will be fitted with leds, and I want to have 3 modes on these, all off, 30% and 100% light.
I want to have one controller/pc that is connected with the first light pole, and hopefully I will be able to have communication between the lightpoles (they will sort of be attached in a string, and not in a mesh or star topology) everytime a car passes a pole the next 10 poles should lite up 100% and the one you just passed will turn down to 30% light.
How many poles can I attach into one system? and if I’m at pole 15 for instance, then this pole should turn on pole 15-25, must this communication go back to the controll and then the controll forward the signals to each pole again?
I want to setup only 5 poles in my system, and they will simulate pole 1,2, 12, 22 and 32 to show the system in action.
Will I be able to do this with a zigbee/xbee system?? What components must I have? and what else do I need??
Could someone help me with this? If I get the system up and running I will also reward the one that help me all the way ![]()
Best regards
student from Norway