hi everyone;
I’m a new comer in MSP430. I’m trying to use interrupt function in port 2 of MSP430f1232 but it didn’t work. My code is below. Can anyone help me, please?
include <msp430x12x2.h>
void delay1s(void)
{
int x = 100000;
while(x != 0) {x–;}
}
void delay1m (void)
{
int y = 60;
while ( y!= 0)
{
y–;
delay1s();
}
}
int main(void)
{
WDTCTL = WDTPW + WDTHOLD ;
P1DIR = 0xFF;
P1SEL = 0x00;
P1IE = 0x01;
P1OUT = 0x00;
P2IE = 0x00;
P2DIR = 0x00;
for (;![]()
{
P2DIR = 0xFF;
P2OUT =0x00;
P2DIR = 0x00;
_EINT(); // Enable interrupt
if ( P2IN == 0x01)
{
P1OUT = 0xFF;
delay1m();
}
else
{
P1OUT = 0x80;
delay1m();
P1OUT = 0x40;
delay1m();
}
}
}
// Port 2 interrupt service routine
__interrupt void Port_2(void);
__interrupt void Port_2(void)
{
P2IN = 0x01;
}
When MSP runs, it checks pin 2.0, if pin 2.0 is high, then it turns on pin 1.6 and pin 1.7 , if not, turns on pin 1.7 and pin 1.6 sequentially. When program runs, e.g during delay1m ( delay 1 minute ), I set up pin 2.0 high level, program should stop running delay1m immediately , jump back in position where _EINT() is. But some thing is wrong and it didn’t work. Can anyone please help me?
Thanks for advance.