Does SFE have an issue with putting a camera connector on ESP32 boards? I now they use up lots of pins but are great for many things.
As this is yet another 3v3 board in the Uno format are there going to be any 3v3 shields?
I have an ESP32 in the RPi zero format that has the camera on one end with the SD card at the other with the 2 x 20 pins. it includes a battery connector and I2S mic. I have tried it it with some RPi hats and it mostly has a Qwiic hat on most of the time. A board in the RPi B+ format with camera connector, external antenna option, and Qwwiic would be great.
Dale