I’m experiencing a strange issue connecting between two Series 2 XBee devices.
One of the XBee devices is mounted on an Arduino Fio and the other is connected to a Windows PC using an XBee Explorer USB.
I have configured the XBee connected to the Windows PC as a Zigbee Coordinator and the Xbee mounted on the Fio as a Zigbee End Point. I have programmed the Arduino Fio successfully using an FTDI cable and have confirmed the receipt of serial data via the FTDI cable.
When I disconnect the FTDI cable, mount the XBee and turn the Arduino Fio on, the XBee fails to connect to the coordinator. However, if I disconnect the FTDI cable, mount the XBee and reconnect the FTDI cable the XBee connects to the coordinator successfully. Once the XBee has connected to the coordinator, I am then able to disconnect the FTDI cable and communication continues. The XBee simply fails to connect to the coordinator when powered by the battery alone. I’m using a 3.7V Polymer Lithium Ion Battery.
Any help you can offer would be greatly appreciated.
Many Thanks