JTAG USB OCD Tiny and Str711

I bought the USB Tiny and the Str711 for modbus development but can’t get Rowley Crossworks or the Eclipse environment to recognize the programmer. I can compile in eclipse and Crossworks but can not download or run or debug the code. I’ve also used the property settings offered by Olimex for the USB Tiny to be used with Crossworks:

nSRST Inversion Mask 0x0200

nSRST Mask = 0x0200

nTRST Inversion Mask = 0x0000

nTRST Mask - 0x0400

Output Pins = 0x0F1B

Output Value = 0x0408

PID: 0x0004

VID: 0x15BA

with no joy. The settings are suppose to be for V1.7 and I have 2.?.

Any fast, if not cheap, suggestions?