Hi there!
After reading the [SparkFun QwiicBus Hookup Guide I still haven’t grasped how to configure my endpoints and my midpoint when the ENTIRE SYSTEM is at 5V.
I have 2 endpoints and a single midpoint in my project. My starting endpoint is powered with 5V at VCC1 originating from my Arduino Nano. Then there is a midpoint with a 5V tolerant sensor connected using a QWIIC cable. Furthermore there is an ending endpoint also with a 5V tolerant sensor connected using a QWIIC cable. That is, I have no need for 3.3V at all.
The following is what I believe I should configure after reading the documentation.
Midpoint
The Bypass jumper on must be OPEN. The PSEL jumper should be set to 1.
Endpoints
The 0-1 jumper on the primary / first EndPoint should be OPEN but the 0-1 jumper on the terminating / last should be CLOSED.
My question is if the above seems correct and is complete. I would prefer not to activate the buck regulator at all since I won’t need the 3.3V for anything but that seems unavoidable. I guess my usage scenario isn’t very uncommon.
Thanks!!! :D](https://learn.sparkfun.com/tutorials/sparkfun-qwiicbus-hookup-guide#hardware-assembly)