k type thermocouple

has anyone used a thermocouple k type with arm or specificaly LPC2148 ?

looking for code or ideas etc , i was thinking of using an AD 595 but wondered if it was realy needed

also looking for hooking up a halleffect to measure RPM ( Tacho )

thanks all

Dave

http://datasheets.maxim-ic.com/en/ds/MAX6675.pdf

Check these out! Pretty sweet. Whatever IC or schematic you choose make sure you use something with cold junction compensation for accurate results.

The MAX6675 senses and corrects for the changes in

the ambient temperature with cold-junction compensation.

The device converts the ambient temperature

reading into a voltage using a temperature-sensing

diode. To make the actual thermocouple temperature

measurement, the MAX6675 measures the voltage from

the thermocouple’s output and from the sensing diode.

The device’s internal circuitry passes the diode’s voltage

(sensing ambient temperature) and thermocouple

voltage (sensing remote temperature minus ambient

temperature) to the conversion function stored in the

ADC to calculate the thermocouple’s hot-junction temperature.

Don’t forget that the voltage out of a Thermocouple is also a non-linear function and must be accounted for (usually by a lookup table).

I’m using AD7708 16bit ADC to measure J and K thermocouples and the ‘cold temperature’ via a thermistor. This gives me pretty good results, but don’t forget that if you need 1ºC resolution, the 10bits internal ADC is not enough, and use of specific IC’s probably will be more expensive.

So if it is a one-off project, better you go with Maxim’s solution, otherwise could be better to use an external ADC and some math.

Guillem.