Hi all,
I’m attempting to recreate the countup timer on the Sparkfun website with my Arduino but I’m having issues. I’ve purchase the large digit drivers and the 6.5" seven segment displays. It appears that any time my leading digit is a 1 or 4, the following digits go haywire.
I’ve tried it with three digits as well, and still, same problem. To visualize, if I create a counter from 0 to 999 with three digits 000-099 work, 200-399 work, and 500-999 work, but the 100’s and 400’s display odd segments including the dp.
If you guys can provide any assistance, it would be greatly appreciated… I’m really going crazy over here.
Thanks!
-Mc
Hi Mc,
That’s a pretty weird issue here. Just to confirm it is not a code issue, have you tried using our [Two-Digit Example Code from the Hookup Guide? If not, give that a try. Also, I’m not familiar with the tutorial you are following, can you provide a link to that in case there is a problem with the code in that tutorial?](Large Digit Driver Hookup Guide - SparkFun Learn)
Give this code a try and see if it works for you. It originally drove a 4 digit display but I’ve modified it so that it should drive a three digit display.
/*
/*
Four daisy Chained Shift Registers that create a 4 digit counter.
74HC595 connected to 7-Segment LED display. The bit order corrosponds to the SparkFun Large Digit Driver
but feel free to rearange your bits if you use a different order.
*/
int dataPin = 7;
int latchPin = 5;
int clockPin = 6;
// Segment letter in a 7 segment display: HBCDEGFA
// Digit to display: 0 1 2 3 4 5 6 7 8 9
// Hex value: 0x7B 0x60 0x5D 0x75 0x66 0x37 0x3F 0x61 0x7F 0x77
byte dec_digits[] = {0b01111011, 0b01100000, 0b01011101, 0b01110101, 0b01100110, 0b00110111, 0b00111111, 0b01100001, 0b01111111, 0b01110111 };
// 0b means binary, 0 is off, 1 is on. We're turning on and off different segments here to create numbers on the display.
void setup() {
//set pins to output so you can control the shift register
pinMode(latchPin, OUTPUT);
pinMode(clockPin, OUTPUT);
pinMode(dataPin, OUTPUT);
}
void loop() {
// for (int thousandsColumn = 0; thousandsColumn < 10; thousandsColumn++) { //First digit (Xnnn)
for (int hundredsColumn = 0; hundredsColumn < 10; hundredsColumn++) { //Second digit (nXnn)
for (int tensColumn = 0; tensColumn < 10; tensColumn++) { //Third digit (nnXn)
for (int onesColumn = 0; onesColumn < 10; onesColumn++) { //Fourth digit (nnnX)
// take the latchPin low so
// the LEDs don't change while you're sending in bits:
digitalWrite(latchPin, LOW);
// shift out the bits:
shiftOut(dataPin, clockPin, MSBFIRST, dec_digits[onesColumn]); //Write out first digit
shiftOut(dataPin, clockPin, MSBFIRST, dec_digits[tensColumn]); //Write out second digit
shiftOut(dataPin, clockPin, MSBFIRST, dec_digits[hundredsColumn]); //Write out third digit
// shiftOut(dataPin, clockPin, MSBFIRST, dec_digits[thousandsColumn]); //Write out fourth digit
//take the latch pin high so the LEDs will light up:
digitalWrite(latchPin, HIGH);
// pause before next value:
delay(100);
}
}
}
// }
}
Thanks for responding TS CHRIS,
Should I use the code you’ve provided to replace a section of the tutorial code? I don’t see a counting variable in there otherwise. I’m sure thats what you meant, but I just want to confirm
Sorry for the last reply Chris. It’s been a long day. I see now how it is supposed to increment.
I’ve discovered that the program as you sent it, counts the time between resets on the Arduino. It does this as a multiple of 10… 1 second represents a 10 count, 10 seconds represents a 100 count and most importantly… it displays the digits correctly.
Now, if I can modify it to work off of a Runtime variable I have… I’ll be set!
TS-Chris:
Give this code a try and see if it works for you. It originally drove a 4 digit display but I’ve modified it so that it should drive a three digit display.
Hi Chris,
It appears to be working, but I can’t get it to display the digits while running. I have to hit the reset button to send it to the digits. What am I doing wrong?
Mc
There might be an error in my code. I’m going to test it and see if I can narrow down what it might be.
Thanks for all your help Chris.
I found that the board has a dead pin. Must have done something to it while experimenting. Anywho, changed the pins and now your code works perfectly!!!
Can you give me some advice on blanking the digits (turning all off)?
Nevermind! For some reason I thought ’ ’ was not an int. everything works! Thanks again!