muntron:
If you breadboard is still attached, you might try an experiment. Set up the display with one LET lit on the first row, two on the second, etc. with 8 on the bottom. Can you see any difference in the brightness of the rows?
I don’t notice any difference with any of the letters I’ve got, so I doubt any difference would be noticed in normal usage. I did try a similar setup a while ago and didn’t see any difference in brightness.
bigglez: In that case, do you suggest I keep on using the shift registers? I’d rather not have them suddenly die, but at the same time I don’t know that I can fit output drivers on?
Alternatively, would [these ([SparkFun] by any more suited? They are larger packages, which might be a pain, but they are also capable of 150mA/channel, 500mA max.
I don’t know if all that would physically fit on the board without going to an SMT version of the uC though…](Shift Register 8-Bit High-Power - TPIC6B595 - COM-00734 - SparkFun Electronics)