Hi,
I’ve problem with LiDAR Lite V3HP.
I can’t measure the velocity with it, cause it’s always returning the 0 value.
Object on which i was doing a tests in quite big and sensor can measure the distance between them, so i guess it is fine.
Do you have any tip why I can get proper value of object velocity?
             
            
              
              
              
            
            
           
          
            
            
              Share the code being used and maybe someone can help out
             
            
              
              
              
            
            
           
          
            
            
              Sure.
I’m using code from [this repository. It’s in Lidar_Lite.py file.
In short I’m using default setting [LiDAR Lite V3HP sensor.
While object in front of sensor is moving, I try to read a velocity from 0x09 register.
Function for reading velocity is:
    def get_velocity(self) -> int:
        """
        The velocity measurement is the difference between the current
        measurement and the previous one, resulting in a signed (2’s complement)
        8-bit number in cm. Positive velocity is away from the device. This can
        be combined with free running mode for a constant measurement frequency.
        The default free running frequency of 10 Hz therefore results in a
        velocity measurement in .1 m/s.
        Returns
        ----------
        int
            Velocity in m/s.
            Positive value is returned when object is moving away from sensor.
            Negative value is returned when object is moving towards sensor.
        """
        vel = self.read_reg("VELOCITY")
        return self.signed(vel)
In my case it’s always returning 0 value.
The speed with which I pass the object in front of the sensor does not matter, and so the reading is 0 .](https://learn.sparkfun.com/tutorials/lidar-lite-v3-hookup-guide?_ga=2.119252361.122531728.1622056494-1162600219.1607511913)](LiDAR-Lite · PyPI)
             
            
              
              
              
            
            
           
          
            
            
              To verify the Lidar Lite is working correctly, can you try connecting it to an Arduino as detailed in our [hookup guide?](LIDAR-Lite v3 Hookup Guide - SparkFun Learn)
             
            
              
              
              
            
            
           
          
            
            
              I already did, as on below picture.
https://cdn.sparkfun.com/r/600-600/asse … ors_bb.jpg
Still I was getting 0m/s.
Might it be due to too fast time sampling? I’m using default setting of a sensor.
             
            
              
              
              
            
            
           
          
            
            
              Sounds like there’s something wrong with your sensor.
If you purchased the sensor directly off our website, just [fill in the form on this page with your order number and the URL to this forum post and we can replace it for you.
If you purchased from a distributor or Amazon you will need to let them know you have a defective product and arrange with them for an exchange.](Return Policy - SparkFun Electronics)
             
            
              
              
              
            
            
           
          
            
            
              Hi, guys,
I found the reason why this is happening.
Well, the LiDAR V3HP does not support velocity measurement, only the LIDAR Lite V3 does.
I recommend to check exactly what type of sensor you have.
I hope this answer will help someone:)