OK, it’s not the end of the world, but line parsing in the command file seems finicky.
Examples -
works - “jtag_device 4 1 0xf 0xe”
doesn’t - “jtag_device 4 1 0xf 0xe”
works - “reset_config srst_only”
doesn’t - “reset_config srst_only”
works - “target arm7tdmi little run_and_halt 0 arm7tdmi”
doesn’t - “target arm7tdmi little run_and_halt 0 arm7tdmi”
I tracked down the parse_line() function in command.c, but it uses an algorithm only a mother could love
, so I haven’t gone beyond that.
If any maintainers are monitoring this board, this might be a quick fix to add to a future release.
Thanks for creating/maintaining OpenOCD!