LM3886 Library - Cannot Connect To Pin 1!

I found two libraries containing the LM3886 - one from a google search (the GainClone library), the other from Eagle’s site. When I add the part to a schematic, I cannot connect a net wire to Pin 1 - it goes to either side of the pin, almost like the pin isnt on the grid.

Link to the libraries so you know what I mean:

http://rapidshare.com/files/180453006/lm3886.zip.html

I don’t use Eagle, but that sounds like the well-known feature/bug with the grid; pins need to be on the grid otherwise you can’t connect to them. They really should have fixed it by now. You probably need to edit the schematic symbol.

Leon

SpikedCola:
I found two libraries containing the LM3886 - one from a google search (the GainClone library), the other from Eagle’s site. When I add the part to a schematic, I cannot connect a net wire to Pin 1 - it goes to either side of the pin, almost like the pin isnt on the grid.

Link to the libraries so you know what I mean:

http://rapidshare.com/files/180453006/lm3886.zip.html

I looked at the LBR’s, and sure enough, the author didn’t have all of the symbol pins on the schematic grid (0.1"). The manual is really clear that a part’s symbol must be on the grid. So while recovering from the flu, and being bored, I decided to fix the symbols in both LBRs (for FREE). I’ve ZIP it, and it’s ready to go. How should I send it to you?

-Dave Pollum

I appreciate all the hard work! Unfortunatley, Im sick aswell, and I played around with Eagle for long enough that I managed to fix them aswell :slight_smile: I created a post with my current project, if you would like to check it out. However, Im sure there are others looking for a proper library, so it definately wouldnt hurt to post it (as yours is likely better than mine)