I have been tweaking my setup for a few weeks now and have it mostly tuned. However, my stepper motors (https://www.oyostepper.es/category-7-b0-Motor-paso-a-paso-NEMA-23.html) are still not behaving as I would like them to. They work fine but I would like to reduce the drastic changes in direction, especially for short lengths of padding.
I have gradually turned the acceleration and jitter down to 750/2.5. In the cura I have reduced the speed to 30mm and 15mm but it is still jarring. Today I upgraded my bracket and coupler so that it can handle it but I really hope it fixes this.
I would like to have it cushion the changes in direction so I can ramp the speed back up. Also, at the start of a move or a line change, the motor will jitter violently and then resume moving smoothly. This is by far the most annoying problem.
Any suggestions would be greatly appreciated.