I’ve got a batch of the latest LoRa serial radios. The pairing method has changed from product 19311 to 20029. Previously you held the train button on each for a few seconds until the LED’s started to cycle, then they matched and displayed full green LED’s showing link established. To pair the newer version I need to hold one until the blue light flashes (server) then hold the other until yellow (client) and then they blink to say the are paired, which happens well and I hear the units reset. During this the server shows:
Server training parameters
Training netID: 154
Training key: 537061726B46756E547261696E696E67
Server radio protocol parameters
netID: 234
Encryption key: 5FBA2B6C39C59F153FC34D888150E0D0
Client 7A6981785730305020312E5026150DFF Trained
And the client shows:
Link trained from 831F9C965730305020312E50031D0FFF
But there is no serial transmission over the link. On the earlier link the radios would now be a transparent link. Am I doing something wrong? I’ve repeated the above sequence several times
I have a brand new pair that work fine out of the box, but we’re not getting anything remotely long range. 100 yards. We’ve tried different settings by AT command, but no improvement. Can you provide example settings that will give us mile-scale connectivity between the pair? Right now, we’re just trying to replicate your online video. Many thanks, Harold
Do you have a clear line-of-sight? How many bps are you transmitting? Run through the settings list here https://docs.sparkfun.com/SparkFun_LoRa … o-commands and maybe try to lower the AirSpeed parameter, you can also increase the timeouts and whatnot
HI… I am trying to test real-world applications, so clear line of site isn’t part of that. Still, I certainly expected something in the order of a mile with neighborhood driving, and it wasn’t close.
I’ll try multipoint and lower AirSpeed with smaller packets and slower retries.
Miles of point-to-point range with VHF or higher is not realistic without elevation and/or clear line of sight like over open water. This is regardless of radio type and signaling technique. Higher power, reduced bandwidth, directional antennas, and digital tricks like error correction can help to a point but structures, vegetation, noise, and terrain blocking the signal path will ultimately prevent the devices from talking.