I am currently facing issues with the LPC 2148 and the UART1. I am using the MAX3232 line driver to connect to the serial port on the PC.
I seem to have shorted the TX and RX pins on the LPC2148 while connecting it to the MAX3232. It serial connection is not working anymore.
IS there a way to find out if the issue is with the max3232 line driver or the LPC2148.
Thanks
Sumit
Use a loopback test, and look at the signals with a scope. That’ll show where the problem is.
Leon
leon_heller:
Use a loopback test, and look at the signals with a scope. That’ll show where the problem is.
Leon
Thank you for your help Leon. I was able to quickly identify thatthe Max3232 line driver is working fine using the loopback test.
But this means that the UART on LPC2148 is too fragile. Is this a general problem and what should I do to eliminate this issue next time. I use the LPC Header board from Olimex.
Best Regards,
Sumit
I’ve not seen anything on the LPC2000 group about the UARTs being fragile, and I’ve had no problems with them on the LPC2148. You might have a bad solder joint.
Leon
leon_heller:
I’ve not seen anything on the LPC2000 group about the UARTs being fragile, and I’ve had no problems with them on the LPC2148. You might have a bad solder joint.
Leon
I tried connecting to the transmitter pin directly an found that it still works. I will try figure out a way to get to the broken female header pin.
Many thank again.