LPC-E2124 default IP adddress and reset blues

Hi,

I just bought an LPC-E2124 (LPC-WEB) board, and it seems to get power from the +5V supplied by the FTDI chip OK. It does seem like the 2124 is not getting a robust reset signal because I have to use the pushbutton reset on the board.

Also, for Olimex, what kind of demo code is running on the board? Is it running a web server at a particular non-routable address (i.e. 192.168.0.1 for example)?

Thanks,

default IP is 192.168.0.30 as in MSP430-EasyWeb

for the reset check JRST state - this should be ON only when download code through Flash ISP utility and open otherwise

BSL jumper should be open to run the code from internal flash

Best regards

Tsvetan