I’m a complete ARM newb/AVR convert, and my LPC2387 is killing me!
I’m just trying to write the simplest possible program (w/ all my own code) as a starting point, but haven’t been able to get that to work yet.
I’m using the WinARM GNU GCC toolchain, and Flash Magic for loading my program over serial to the bootloader.
I basically just have the startup code in assembly, and a single-pin toggling main function in C (but the LED ain’t flashing…).
Can anybody guess where I’m going wrong here? TIA!! ![]()
LPC2387.S
.text
.arm
.extern main
.global _start
_start:
//=====================================================
B INIT // Reset
B LOOP // Undefined Instruction
B LOOP // Prefetch Abort
B LOOP // Data Abort
NOP // Bootloader Checksum
B LOOP // Interrupt Request
B LOOP // Fast Interrupt Request
//====================================================
INIT:
LDR R3,=BASEADDR
// Disconnect PLL
LDR R0, =0
STR R0, [R3, #PLLCON]
LDR R0, =0xAA
LDR R1, =0x55
STR R0, [R3, #PLLFEED]
STR R1, [R3, #PLLFEED]
// Set Clock Source to Main Oscillator
LDR R0, =1
STR R0, [R3, #CLKSRCSEL]
// Wait for Main Oscillator to Settle
OSC_LOOP:
LDR R0, =0x1A0
ANDS R0, R0, #0x40
BEQ OSC_LOOP
// Switch from Internal Clock to Main Oscillator
LDR R0, =0x1
STR R0, [R3, #CLKSRCSEL]
// Setup PLL Scalars
LDR R0, =0x001000BF //((16<<16) | 191) == 0x001000BF >> (12*2*192)/16 = 288 >> /4 = 72MHz
STR R0, [R3, #PLLCFG]
LDR R0, =0xAA
LDR R1, =0x55
STR R0, [R3, #PLLFEED]
STR R1, [R3, #PLLFEED]
// Enable PLL
LDR R0, =1
STR R0, [R3, #PLLCON]
LDR R0, =0xAA
LDR R1, =0x55
STR R0, [R3, #PLLFEED]
STR R1, [R3, #PLLFEED]
// Set CPU Clock Divider (to 4)
LDR R0, =0x3
STR R0, [R3, #CCLKCFG]
// wait for PLL to stabilize
LDR R0, =0x4000000
PLL_LOOP:
LDR R1, [R3, #PLLSTAT]
ANDS R1, R0
BEQ PLL_LOOP
// Connect PLL to CPU
LDR R0, =0x3
STR R0, [R3, #PLLCON]
LDR R0, =0xAA
LDR R1, =0x55
STR R0, [R3, #PLLFEED]
STR R1, [R3, #PLLFEED]
// Stack Pointer */
LDR SP, =0x40010000
// Main
BL main
LOOP:
B LOOP
main.c
#include "LPC23xx.h"
int main(void)
{
int i; //attempting to toggle P0.16 here
IODIR0 = 0x00010000;
PINSEL1 |= 0x00000003;
while(1)
{
IOCLR1 = 0x00010000;
for(i=0; i<6000000; i++) ;
IOSET1 = 0x00010000;
for(i=0; i<6000000; i++) ;
};
}