Is there a software for programming LPC2106, LPC2138 micros under linux (through serial port)?
I’m looking for an equivalent of the LPC200 flash utility
Is there a software for programming LPC2106, LPC2138 micros under linux (through serial port)?
I’m looking for an equivalent of the LPC200 flash utility
Look at lpc21isp. It’s what I use, and it works just fine.
Alex
Thanks for the reply ![]()
Do you know where can I download it?
Is it available in .deb or .rpm file or it’s just a C file to compile & use?
Is it command line or gui?
I used the one from here:
http://www.lumme.fi/code/c/lpc21isp/
Just compile and go. It’s got a CLI, so it may not be what you’re used to, but it works great.
Alex
thanks for the link
no problem for the command line interface, it’s even better, so I can call lpc21isp from the makefile 8)
I’ll do something like
make all //to compile
make program //to call lpc21isp and upload file to the microcontroller