LPC2103 Scanning multiple ADC ?

Hello,

I am newbie. I can sucessfully scan one channel but dont know hot to scan multiple ADC channels ? Can some one please help me with some examples ?

I will really appreciate the help.

Cheers,


unsigned int val; // ADC Result (HEX)

float volt; // ADC Result Volt

int main(void)

{

init_serial0(); // Initial UART0 = 9600,N,8,1

printf(“ET-ARM7 BASE LPC2103…TEST ADC-0(P0.22)\n”); // Call prinff Function

// Initial ADC0 (GPIO-0.22) By Set PINSEL1[13:12=11]

// xxxx xxxx xxxx xxxx xx11 xxxx xxxx xxxx

PINSEL1 &= 0xFFFFCFFF; // Select ADC0 Pin Connect P0.22

PINSEL1 |= 0x00003000;

// Initial ADC0 (ADCR=0x01210601)

ADINTEN = 0; // Disable ADC Interrupt

ADCR &= 0x00000000; // Clear All Bit Control

ADCR |= 0x00000001; // Select ADC = AIN0

ADCR |= 0x00000600; // ADC Clock = VBP(PCLK) / 7

ADCR |= 0x00010000; // Busrt = 1 = Conversion Continue

ADCR &= 0xFFF1FFFF; // CLKS = 000 = 10Bit : 11 Cycle Clock Conversion

ADCR |= 0x00200000; // PDN = 1 = Active ADC Module

ADCR &= 0xFF3FFFFF; // TEST[1:0] = 00 = Normal Mode

ADCR &= 0xF7FFFFFF; // EDGE = 0 = Conversion on Falling Edge

ADCR |= 0x01000000; // START = 001 = Start Conversion Now

// Start Test Read ADC0 and Display on UART0 //

while(1) // Loop Continue

{

do // Loop Read ADC0

{

val = ADDR0; // Read A/D Data Register

}

while ((val & 0x80000000) == 0); // Wait ADC Conversion Complete

val = (val >> 6) & 0x03FF; // Shift ADC Result to Integer

volt = val * 3.3 / 1023.0; // Volt = ADC Result x [3.3V / 1024]

printf(“\rADC0 Result = %1.1f Volt.”,volt); // Display 3-Digit Result(0-3.3V)

delay(10000);

}

}