Hi all,
I’m not whether this would make sense asking this question here or in the robotics section, but this is more of a programing question than anything else. I’m trying to make 4 IR sensors map out different values to command a servo motor to turn certain degrees 2 of the IR sensors store a value for the left side, and 2 store a value for the right side. What I want to happen is that when the IR sensors pick something up between 25 inches and 5 inches, it turns the servo a certain amount of degrees based on how close/far an object is. I have the code for the right side working alright, but it doesn’t make sense to why it works. I’ve tried doing the left side with mixed results but none that I want. The basic code is below, full code is attached–can anyone help?
if(Prox01 <=25)
{
leftSide = Prox01;
leftSide = map(leftSide, 5, 25, 130, 95);
Steering.write(leftSide);
}
That one works, while below does not.
else if (Prox04 <=25)
{
rightSide = Prox01;
rightSide = map(rightSide, 5, 25, 65, 95);
Steering.write(rightSide);
}
More information on my robot is here:
http://letsmakerobots.com/node/35388
Thanks!