Hi
I have an issue with my Max M10S connected over I2C.
I believe it maybe an issue with the library and have posted it I2C held up for over 1sec · Issue #62 · sparkfun/SparkFun_u-blox_GNSS_v3 · GitHub
Basically the first function of the library I call takes over 1000ms holding up the I2C and stalling the processor for this time.
All subsequent library functions run in 0ms untill the loop is re-run.
As such all other processes are preventing screen refresh and other bits of my code. I would appreciate if someone could help
             
            
              
              
              
            
            
           
          
            
              
                PaulZC
                
              
              
                  
                  
              2
              
             
            
              Hi David,
Please see my reply on GitHub for the answer:
Best wishes,
Paul