I am unable to get the internet clock working. The mbed-LPC 1768 mbed light keeps blinking after I press the restart button (as if the code is still running and the graphic LCD display shows the following.
4D Systems
uLCD-144-G2
SPE2 rev 1.3
PmmC rev 2.6
Comms 9600
4D Systems (c)2014
Please note that I imported the libraries and the code copied and pasted from the experiment compiled successfully.
I connected the ethernet cable from the MagJack Breakout to the router.
When I copy and paste the code for the experiment it compiles but there are a number of warnings.
When I copy the code over to the mBed and press the restart button I get a “Waiting…” and then a “Connected!” but the Graphic LCD does not show keyboard input.
I have included a screenshot of the warnings and a picture of the circuit.