Measuring distance to liquid surface

Could a VCSEL or any other sensor be used to precisely determine the distance from the sensor to the surface of water or another liquid?

For example, if the sensor was oriented downward above an open vessel containing a liquid, could it accurately indicate, in millimeters (mm), how far away the water is? Assume here that the water is still/calm and that the maximum distance would be 100 or 200 mm.

Yes you can. You can even use HCSR04 for this purpose.