hello everybody ![]()
i have a little problem with IAR for building my application,
when i have this following error , i decrease the size of the stack (in options => general => stack/heap) and it works
(hoping no “stack overflows”)
" 1 826 bytes of CODE memory
68 bytes of CONST memory (+ 4 bytes shared)
79 bytes of DATA memory (+ 19 bytes shared)
Errors: none
Warnings: none
Linking
xlink.exe D:\IAR_project\Debug\Obj\main.r43 -o D:\IAR_project\Debug\Exe\test_I2C.d43 -ID:\IAR\430\LIB\ -f D:\IAR\430\
CONFIG\lnk430F2013.xcl -D_STACK_SIZE=64 -rt D:\IAR\430\LIB\CLIB\cl430f.r43 -D_HEAP_SIZE=0 -s __program_start
Error[e16]: Segment CSTACK (size: 0x64 align: 0x1) is too long for segment definition. At least 0x33 more bytes needed.
The problem occurred while processing the segment placement command “-Z(DATA)CSTACK+_STACK_SIZE#”, where
at the moment of placement the available memory ranges were “CODE:24f-280”
Reserved ranges relevant to this placement:
200-243 DATA16_I
244-24e DATA16_Z
24f-280 CSTACK
Build aborted. "
But i have nearly the same error now and i do not know what things to change in order to make it work
"
Error[e16]: Segment DATA16_ID (size: 0x44 align: 0x1) is too long for segment definition. At least 0x14 more bytes
needed. The problem occurred while processing the segment placement command
“-Z(CONST)DATA16_C,DATA16_ID,DIFUNCT,CHECKSUM=F800-FFDF”, where at the moment of placement the
available memory ranges were “CODE:ffb0-ffdf”
Reserved ranges relevant to this placement:
f800-f82f CSTART
f830-ffaf CODE
ffb0-ffdf DATA16_ID
Build aborted. "
Do you think that my application is too big ???
Do i have to change the memory map (if i could) ??
thank you in advance for any piece of advice ![]()
baze