Micrium TCP/IP StacK

Hello,

We are using Micrium’s TCP/IP stack and are having a problem. Scenario:

  • Code running on an IAR STR912 dev board which is connected to LAN through the ethernet connector.

  • Code compiled using IAR tools

  • PC, also on lan, used to ping IAR board.

  • ICMP Ping replies come up in < 1ms

  • ICMP Ping reply <1ms maintained indefinitely if LAN consists only of PC and IAR board

  • If connected to large LAN with broadcasts, Ping response time suddenly starts to exceed 1ms after a while…builds up higher and higher to be over a second…and then after a while, the whole MCU freezes.

Has anyone else seen this? Any help will be appreciated!

Thanks

Nirosh