Can we get 12 bits parallel output from FlexIO based on this combination? In other words, are there 12 consecutive FlexIO pin from the combination of MicroMod Teensy+ ATP carrier?
It looks like while there are 12 GPIO you could use they are NOT sequential
From the HW overview of the Teensy MM guide
" General Purpose IO pins
- G0 - Teensy pin 40, MicroMod pad 40
- G1 - Teensy pin 41, MicroMod pad 42
- G2 - Teensy pin 42, MicroMod pad 44
- G3 - Teensy pin 43, MicroMod pad 46
- G4 - Teensy pin 44, MicroMod pad 48
- G5 - Teensy pin 45, MicroMod pad 73
- G6 - Teensy pin 6, MicroMod pad 71
- G7 - Teensy pin 9, MicroMod pad 69
- G8 - Teensy pin 26, MicroMod pad 67
- G9 - Teensy pin 32, MicroMod pad 65
- G10 - Teensy pin 33, MicroMod pad 63
- G11 - Teensy pin 27, MicroMod pad 8"
:-/
But! This thread make me think they don’t need to be sequential? Not certain