got following error when running script
Error: fileio.c:79 fileio_open_local(): couldn’t open xscale/debug_handler.bin
I guess it was after
“target xscale big reset_init 0 ixp42x”
may be I missed something in configuration procedure?
this .bin does not seem to appear in driver directory or compiled?
config script is below as well as openocd responce
#daemon configuration
telnet_port 3333
gdb_port 4444
#interface Olimex OpenOCD–[begin]
interface ft2232
ft2232_device_desc “Olimex OpenOCD JTAG TINY A”
ft2232_layout olimex-jtag
ft2232_vid_pid 0x15ba 0x0004
jtag_speed 16
jtag_ntrst_delay 200
jtag_nsrst_delay 400
#use combined on interfaces or targets that can’t set TRST/SRST separately
#reset_config trst_and_srst srst_pulls_trst
reset_config srst_only
#reset_config trst_and_srst trst_pulls_srst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 7 0x1 0x7f 0x7e
#target configuration
daemon_startup reset
#target
target xscale big reset_init 0 ixp42x
full list of openocd responce is below
Open On-Chip Debugger 1.0 (2008-06-27-21:3 svn:725
Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x29274013 (Manufacturer: 0x009, Part: 0x9274, Version: 0x2)
Info: jtag.c:1389 jtag_examine_chain(): JTAG device found: 0x29274013 (Manufcturer: 0x009, Part: 0x9274, Version: 0x2)
Error: fileio.c:79 fileio_open_local(): couldn’t open xscale/debug_handler.bin
User: target.c:450 target_process_reset(): Timed out waiting for halt afterreset