I’d really like to see a small (tiny) breakout board for the MN5010HS. This thing is tiny and I’m a bit reluctant to dive into a project right now without a little PCB to solder it to. I’m not asking for a USB interface or anything like that… just a simply PCB that accepts the MN5010HS and brings it out to standard .1 headers. Thanks…
If this ever comes about (which I wouldn’t mind seeing), it’d be really convenient to have circuitry on the breakout board to interface 3.3V to all the 1.8V signals.