Hi everyone,I will try to make this question as clear as possible with all necessary information. Please feel free to ask if you require any clarifications. ![]()
I am attempting to control a high voltage motor, the motor itself as well as all other components except for two buttons will be hidden from the user. (I did not select the motor yet but lets say its a 12V DC motor).
So, first off, I was thinking of using an h-bridge such as this one : 1) https://www.amazon.ca/Controller-H-Brid … B00CAG6GX2
The H-bridge shown above can accommodate for a 12 V DC motor which is perfect. Also I can use the 5V output from the H-Bridge to power the Arduino! Win-win.
Okay this is the trickier part. This whole system needs to be placed in a unit that can be powered from a wall outlet. My problem is, a wall outlet is AC and I require DC, also the voltage is much greater that the 12V I require.
So, how would I go about giving the H-bridge a 12V input from a wall outlet?
I know a rectifier could convert from ac to dc and lower the voltage. Here is a unit I found that looks promising, I know the amperage output is too high but its just an idea : 2) https://www.xppower.com/Product/ECP150-Series
My major bump in the road is how to connect a 3 prong wall outlet to a unit like the one found at the link right above this line which I am guessing requires jumper cables or some similar type of connection. Here is a 3 prong wall plug-in in case someone is not sure what it is :
What do you suggest I should do for a system? Is a rectifier module like the one shown at link 2) a good idea? Is there an adapter that would allow to go from 3 prong to some type of connection for such rectifier modules?
Thank you in advance for your input it is great appreciated! I hope this was simple to understand ![]()