Hi, I’m building a very simple turntable using a worm gear (see attached image of a similar worm gear box).
I just need the turntable shaft to turn slowly. That is why I’m using a 30:1 worm gear setup. I need to power this unit. I need to control the speed but I do not need the turntable to find an exact position, although it might be helpful to program it to do so.
I’m looking at stepper motors and DC brushless motors. I need the motor to do the following:
-
to turn at speeds I specify (various slow speeds)
-
low noise, smooth operation.
-
No load to very low load. I’m basically placing a mirror on the shaft of the work gear box. No belts or heavy weights. just a slowly turning 1/4 D shaft. Therefore, I need very little torque.
Although I’m not opposed to using an arduino with a potentiometer, I would rather control the motor with the simplest PC software to change the RPM as needed.
Second, once I get help with the motor selection I would like that motor to connect with a motor driver and the proper controller. As I said above, I would like to use a very simple PC program (I have not found a program yet) to control the speed of the motor.
I’m thinking a motor controller with a USB port to connect to a PC driving a simple motor that I can make turn slowly.
Any help is greatly appreciated. Dwane