I have several ideas for a computer case mod I am working on, and am trying to determine the feasability. Out of all the places I’ve visited, this seems to be the best resource for the level of customization I’m working in. Many case mods are very in depth, but I’m a bit different in the type of mod I’m doing. Many have said it’s akin to ‘putting the Batman suit on a computer’, and I wouldn’t say that’s far off. I’ve browsed the internet for 3 years while I’ve developed this idea, and tried to squirrel away finances, and no one has done anything like this, so I’ll reveal things as needed. I want to retain my idea before others copy it after.
One of the two ideas I have for a secure way to access my computer using biometrics is to hide away a fingerprint scanner. One idea was modifying a drive bay, which is fairly easy in the end, except for programming that scanner, but that’s later. My idea here i’m working on is a push button roll top cover. Basically, I push a button, and a servo turns a cog with the roll top slats on it to roll it back, revealing the scanner, and possibly a near laser for flair. Again, that would be later after i get the basics functional.
For the roll top, my first idea was dissecting an old cd-drives motor and control and just reversing the controls. So, instead of the motor rolling out a drive when the button is pressed, it rolls back the slats. Like a roll top desk ![]()
Reading on here, it appears I might be better served getting the components from here and doing it myself. So, I would need a control board for the basic instruction set, a motor, basic wiring where needed, the cog attached to the motor, and track attached to slats.
How feasible does this seem? Compared to some projects, it seems fairly elementary, but it’s all Greek to me, so I’m searching out help.
There would be low resistance on the track and I would use the best quality bearings on the track slide so as to not stress the motor. The slats shouldn’t weigh much, but I don’t have a weight yet. IF i can match the rest of my case, the slats will have a santoprene skin on them.