MSP430- PIR and MSP430 -JTAG [ Olimex]

Hi,

I have purchased the MSP430-PIR module and MSP430-JTAG from sparkfun. I want to modify the firmware provided by ti.com for the application. I am not able to download the firmware to the MSP430f2013 in the PIR module using the JTAG connector. I am using IAR compiler.

Error message says - Emulator - “No device found …”

Any suggestion would be appreciate.

Thanks in advance

Have you installed the drivers?

Leon

Hi Leon,

Thanks for your reply. I have installed the drivers. I also did test the MSP430-PIR board even by changing the jumper settings but nothing seems to work.

It is not able to detect the MSP430.

Thanks,

Which JTAG are you actually using?

Leon

I am using the Parallel port programmer from sparkfun

http://www.sparkfun.com/commerce/produc … ucts_id=15

I thought you might be using one of the USB units. It should just work, you don’t need drivers for it.

Leon

Thanks…i will get an USB Jtag for programming

The parallel jtag programmer doesn’t support spy-bi-wire. You’ll need at least the msp-jtag-tiny to program via spy-bi-wire.

I have http://www.olimex.com/dev/msp-pir.html

and jtag-rf from olimex:

http://www.olimex.com/dev/msp-jtag-rf.html

but I cant make connection!

??

I test MSP430_JTAG-RF with MSP430-1121STK2 and work ok!

So Jtag-rf working ok…