MSP430FG4618 Failed to write memory at 0x3102

Hi All,

I received the following error while trying out the “Flashing the LED” example that comes with IAR Embedded Workbench for MSP430 V3.41A:

“Failed to write memory at 0x3102”

The following are the steps to reproduce:

  1. Install IAR Embedded Workbench for MSP430 V3.41A

  2. Set FET as the power source jumper on TI MSP430FG461x/F20xx Experimenter’s Board

  3. Connect MSP430-FET430UIF to JTAG1 interface on TI board

  4. Start Embedded Workbench, open “Flashing the LED” workspace in example folder

  5. Set MSP430x4xx as active project

  6. Select Project->Options->General Options->Device->MSP430FG4618

  7. Select Project->Debug

  8. At this point, I will receive the following dialog box:

http://www.imagehosting.com/out.php/i1027515_dlg1.jpg

  1. I choose yes, and I will receive the following error box:

http://www.imagehosting.com/out.php/i1027514_dlg2.jpg

Everything else is basically left untouched. Is there anything I am missing here? The other processor (F2013) is running fine with the same example. Your help will be greatly appreciated.