I’m about to begin an audio project and have zero experience
working with sound cards and such. I am planning to have three
microphones on a set of Mandalorian armor, two microphones on the
outside attached to single speakers inside my helmet (so I may retain stereo style
hearing) and one microphone inside my helmet to broadcast to a speaker
outside the armor.
I was wondering if there is a card that could handle all three of the functions in one, or if I would have to have three separate cards to function each microphone/speaker combination. I am also trying to find something closer to an omnidirectional microphone and I’m concerned that the microphone I’ve added will not suffice. I have currently added the
following cards and microphones to my shopping cart as well as various supporting parts from a tutorial I found.
3X SPARKFUN ELECTRET MICROPHONE BREAKOUT [1]
In stock [2] BOB-12758
3X TEENSY 3.2 [3]
In stock [2] DEV-13736
3X TEENSY PROP SHIELD LC [4]
Only 10 left! [2] DEV-13996
Side not, for now the use of the microphone and such will be with dials, but eventually I will want to hook up the system to a Raspberry Pi Single board computer so I can run everything from my gauntlet computer.