I followed the example for the MAX31855K breakout board with the arduino pro mini on the Sparkfun page, and with one MAX31855K I could read the temperature. However I would like to add in another MAX31855K breakout board to the setup. I have tried a few different ways, but it doesn’t seem to work. Is it possible to have 2 MAX31855K temperature boards on one Arduino Pro Mini using most of the example code on the Sparkfun MAX31855K page?
Can you share a picture of your setup?