Multiple PRT-13813

I would like to make a battery pack that would consist of multiple PRT-13813 to increase capacity and max discharge rate while maintaining the same length and width dimensions but . If I wire multiple PRT-13813 batteries, would that increase the maximum discharge rate as well?

Thanks!

Mike

Hello Mike.

Yes, you can parallel these batteries to increase the max discharge rate. Just make sure that all batteries are fully charged before connecting them in parallel to prevent excessive current from flowing between batteries. Once paralleled, all the cells will stay at the same voltage.