Multiple Trace Width Nets...

Without manually routing or using something akin to an GND-AGND junction to split up nets, is there a straightforward way to have different trace widths on different legs of the same net in Eagle?

I have a number of high current traces that also need to supply a small amount of current to a handful of components… and it’d be nice if the low power traces weren’t super-sized.

You should be routing a board like that manually, anyway.

Leon

While I agree with Leon, if you MUST use the autorouter, you can manually route the high current traces and then let the autorouter do the remaining.

You can also use change/width to change specific traces after they’ve been routed.