hello! I’m quite new here, but not all to new to electronics.
why I am making a PCB (sorry it’s so long, I got carried away. optional read):
I’ve played around with arduinos, breadboards and veroboard, and I have made some fun circuits, but not all to much.
recently I made a breadboard “knight rider” where the LEDs create a left-right swaying pattern, with 5 LEDs, a 555 and 4017. my dad actually got quite interested in this, and wanted it in his car. one problem: I only have one extra large breadboard that I happened to make the circuit on, and even if I rebuild it on another it is all to easy for those connections to come loose.
I wanted to do it on veroboard, but I didn’t for these 2 reasons:
-
I’m…not to good at planning veroboard circuits, and this looks pretty complex.
-
for some reason, on every veroboard project I do there is at least 1 soldering-related thing that goes wrong, leaving me debugging for quite a while. I have heard that PCBs are much easier to solder, and I have soldered headers to those shields without problem. for example, while I had about 3 hard-to-notice bridges on my 2nd veroboard project, a blinking light, I had none on that joystick shield kit witch I soldered months before.
lastly, I wanted to try PCBs. I don’t know why, but I always wanted a custom printed board since I started my hobby. they just seems so professional and fancy. and compact!
the actual questions:
the 4017 in eagle seems to not have VCC or GND pins. the 555 does. if I make those VCC and GND components, are they automatically linked to the 4017 GND and VCC? because I think I’m doing something wrong there. those 2 pins are not connected in the PCB view. do I need a specific set of VCC and GND things?
is “tplace” also top silkscreen? I just want to write something on the board. I can’t find “tsilk” or something in that list.
is 0.125984 the normal size of a screw for making holes? it’s the highest eagle can go, yet it still seems quite small. well it’s probably not the highest, but it’s the highest in the drop-down menu.
lastly, did I make any “obvious” mistakes here? you can also see the disconnected pins n the 4017.
http://i.imgur.com/TNcOt.pnga few more notes:
the power switch is external from the board and connects to the battery.
I know the resistors and cap do not have a value, I’m still going to play around with the speed I want.
the external LEDs are on a veroboard circut I made. the pins go to a little plug and wire, and at the end are 5 resistors and 5 LEDs, sharing ground.